Add Images to a Comment

You can add images that support your comment.

About this task

A comment can have multiple images. You can add images to a comment by uploading them as documents, or taking a screenshot using the camera icon.

Procedure

  1. Select .
    Note:
    If a message appears, asking you to allow access to the camera, select Allow.
    A screen appears in camera mode.
  2. Point the camera to the subject, and select the shutter icon to capture a still image.
    A preview of the image appears in the comment rich text editor along with its filename label, and simultaneously saved to the database.
  3. Optional: To modify the captured image, select the image preview to open the image in an edit mode.
    1. Use the image editing options to resize or modify the image.
    2. Select Save.
    To delete saved images from a comment, delete the image preview or its filename label in the editor.