Skip an Operation

About this task

You can skip an operation that is configured as optional.

Before you begin

  • If you do not have the permission to perform this task, a message appears, stating the same. In such case, request your administrator to provide the permission using Security.
  • You can only skip an operation that is configured as Optional. You can specify an operation as optional using Route Editor.
  • Ensure that the optional operation is in Ready status.

Procedure

  1. In the Work Queue page, in the row containing the optional operation that you want to skip, select the SKIP button under COMP/REC column.
    Alternatively, you can select the operation and work order combination from the Work Queue page, and then select the SKIP button in the page heading.
    Note:
    You can identify an operation as optional using the OPT column. You can add the OPT column using .
    The Select Serial number(s) to Skip window appears displaying all the serials/lots of the operation that are in Ready status.
  2. If you want to skip all the available serials/lots, select the check box in the heading row of the table. If you want to skip specific serials/lots, perform one of the following steps:
    • Select the check box for each serial/lot that you want to skip.
    • Search for a serial/lot by entering the value in the Search in available serial numbers box, and then select the check boxes from the filtered list that appears.
    • Scan the bar code of the serial/lot by selecting .
  3. Select the Skip button to skip the operation.
    The selected serials/lots are skipped.