Chart Header Global Actions
Charts Header Global Actions
The icons ,
, and
, on the chart name in the chart header control the actions across the entire Charts module.
Create Case
To create a case, while viewing charts, select in the Chart Parameters pane.
A window appears allowing you to add the details to the case. This window displays the same fields as when editing an existing case. The meanings of these fields are described in the following section. Required fields are highlighted in yellow if a value is not provided, and the Create Case button is disabled until all required fields have values.
Provide values for all required fields, and then select Create to create the case. Once created, the Charting view changes from the alert charting view to the case charting view and the case () appears in the Tag Browser under the Cases section and will also be available in the Cases module.
Chart Settings
The Chart Settings () allows you to control how your tag date is presented in the chart view.
Chart Setting | Meaning |
---|---|
DATA SELECTION BY
| You can enable point mode for SmartSignal charts, allowing the x-axis to display the number of data points selected instead of a date-time range. In this view, you can select the x axis to display date, time, or points. |
DEFAULT CHARTS
| You can select the standard chart types to be displayed. |
TIME SERIES
| You can select the type of data series to be displayed on the chart. |
MARKER VISIBILITY
| You can select the alert and data quality indicators to be displayed on the chart. |
THRESHOLD SETTINGS
|
|
GENERAL
|
|
Tag Browser Access
The Tag Browser Panel access () allows you to hide and show the panel. The Tag Browser allows you to find tags, view cases, alerts, asset, and tag information. You can select the tags you need to plot from the Tag Browser.