Tag Browser

About Tag Browser

The Tag Browser opens as a panel on the right side of the chart view. Select to hide and show this panel. The Tag Browser allows you to find tags, view tag information, and plot tags.

The Tag Browser loads the in-context asset and its associated tags by default. You can add additional assets and their associated tags to the Tag Browser.

You can plot Asset and Model tags from the Tag Browser.

The Asset node in the Tag Browser expands to display each mode node. Each mode node expands to each model node. Each model node expands to show the input and output tags. To view the tag details in a tool tip, click over a tag in the Tag Browser. Tool tips are not available for nodes.

Use the Tag Browser to:

  • Plot tags to the charts for the selected view.
  • Access tag information.
  • Add and remove multiple assets and their associated tags.
  • Search the Tag Browser by tag name.

Nodes and tags listed in the Tag Browser appear with specific icons depending to help with quick visual recognition:

Tag IconMeaning
Case
Tag
Tag contributing to an alert
Asset
Asset containing an alert
Calculated or Output tag.
Note: If you hover over the calculator icon, a detailed tool-tip will display contain information about the tag. The tag expression will be included if the user has been granted permission by the system administrator.
Calculated or Output tag that is contributing to an alert
Group of tags
Group of tags containing an alert
An Alert that has a status of New
An Alert that has a status of Investigating
An Alert that has a status of Assigned
An Alert that has a status of Acknowledged
An Alert that has a status of Deferred
An Alert that has a status of Escalated
An alert that has a status of Retrain Deferred

About Cases

Under the Cases () section you can see the list of every case that is open against the parent asset that you are viewing. Under each case there is a list of alerts that have been linked as evidence for the case. You drag and drop the entire case into the charting area to view all the tags associated with the case.

About Asset

Under the asset () section you can see the tags grouped by mode, model, tags on monitor, and analytic tags. You can drag and drop any of the groups into the charting area to view all the tags associated with the asset.