Global Chart

Global Chart Date and Time Zone Selection

The chart date and time zone controls allow you to customize the data that you see in your charts.

Simply use the calendar controls to select the time range, then optionally you can specify the time zone if you prefer to view using UTC or Asset Local Time, instead of the default (i.e. your user time).

Global Chart Action Controls

The following icons allow you to perform actions across all the charts that currently in your chart view.

IconGlobal Chart ControlDescription








Zoom Across x-axis

Zoom Across y-axis

Zoom Across both x-axis and y-axis

Reset Zoom

  • When you zoom on the charts, the chart will zoom into the points selected on the chart and optionally the Y axis range if you have selected an XY zoom.
  • All the other charts in the card will also zoom into the same points and the X axis on the charts will show the point numbers that you have zoomed into.
  • When you reset the zoom on the charts, all the charts will return to their normal points range and values as they were before you zoomed into the charts.
Resize ChartYou can control the size that your charts appear:
  • Small
  • Medium (Default)
  • Large
  • Largest


Pan ChartPanning allows you to move through the chart data left and right, maintaining your current zoom level.
Toggle all residual chartsAllows you to easily hide/show the residual charts of any modeled tag being displayed in the chart view area.
Compare AssetAllows you to select an asset derived from the same blueprint to overlay their values onto the original asset.
  • Delete All Charts
  • Delete Hidden Charts
  • Clears all the charts currently displayed in the chart viewing area.
  • Clears the charts currently hidden in the chart viewing area only.