First name
Sawan
Last name
COEME GILLARD

Member for

1 year 5 months

Case Studies

SFC for railway traction power supply in Bauhinia

February 25, 2025

In 2014, GE Vernova’s Power Conversion & Storage business delivered and commissioned the SFC systems for the Bauhinia electrification project in Australia. It was the very first time that power electronic converters were employed to feed a 50 Hz electric railway.

System Overview

The project encompassed two independent feeder stations, each featuring a 19 MVA converter system based on Power Conversion & Storage’s proven MV7000 converter technology

These converters are housed within a transportable substation building, which includes a control room, while additional supporting equipment is located externally.

A single converter block comprises the following main components:

  • Input 3-phase 4QS sub-inverter with three single-phase modules
  • DC link with an extensive capacitance
  • Output 1-phase 4QS sub-inverter with two phase modules 

The core components of each sub-inverter are the press-pack IGBT modules, arranged in two phase segments and equipped with a patented pull-out mechanism, including the IGBT control amplifiers.

World's first application of 50-50Hz rail static frequency converters

SFC system details

Transformer

The design of the converter system necessitates the installation of two transformers for each converter block. Both transformers are designed for outdoor use and feature an ONAN cooling system, tailored for the hot weather conditions of Queensland, Australia. The input transformer, rated at 132 kV and 50 Hz, has three output windings that directly supply the three inverter units. The output transformer increases the converter’s single-phase 16.5 kV output voltage to supply the railway with a ±25 kV, 50 Hz power. A railway filter is connected to both the output of the railway transformer and its auxiliary winding.

Cooling system

Each converter block features its own dedicated cooling system, using a glycol-water mixture to directly cool the power electronics. The cooling system is designed to operate in temperatures up to 45 degrees Celsius and includes an enhanced water-air heat exchanger to manage the minimal temperature difference between the ambient air and the required inlet fluid temperature. Two water pumps are installed with complete redundancy to ensure continuous circulation, with the pumps alternating every 24 hours. Additional air conditioning is provided for the station premises.

Control system

The internal converter control system facilitates the following operational modes: 

  • Standard control in all four quadrants,
  • Phase shift operation (supplying reactive power solely to the railway grid),
  • Parallel operation with the existing standard 50 Hz railway feeding system,
  • Isolated mode (establishing its own railway grid).

The control system can be operated locally or remotely through a user-friendly HDM interface.

Circuit diagram of the SFC

Proven expertise and local support

Opting for Power Conversion & Storage’s SFC technology offers several benefits:

  • An unparalleled blend of proven static frequency converter technology, extensive global rail expertise, and localized support, including engineering, project management, and service,
  • High efficiency and low operating costs,
  • Single output transformer,
  • High availability, due to a modular design and high degree of standardization,
  • IGBT design optimized for highly dynamic loads,
  • Maintenance-optimized design,
  • Short commissioning time,
  • Scalable concept.

Technical specifications

Technical specifications of the SFC