A more reliable, flexible, and resilient Vietnam
Powered by high-efficiency gas turbine technology
Supporting economic growth in Vietnam
With experience through decades of global heritage, GE Vernova offers a full spectrum of gas power technologies engineered to help Vietnam meet rising electricity needs with greater efficiency, flexibility, and resilience. From large-scale combined-cycle plants to fast, modular power solutions, our gas turbines are well-positioned to support the country’s evolving energy mix—providing more reliable baseload power while enabling greater integration of renewables.
Among our most advanced offerings are the H-class and aeroderivative gas turbines, each with the capacity to play a distinct role in shaping a more sustainable and dependable energy future.
Cost-effective power
As Vietnam’s economy grows and electrification expands, the need for more reliable, affordable baseload power becomes increasingly urgent. With more renewable energy entering the grid, always-available generation is essential. That’s where heavy-duty gas turbines come in—helping to deliver high-efficiency power, with reduced fuel to power cost conversion—supporting the country’s long-term energy goals.
More reliable power—with less spend
GE Vernova’s HA gas turbine fleet is engineered for high-class efficiency, performance, and scale. With the lowest cost conversion of fuel to power in the conventional industry, the HA fleet generates more electricity at a lower cost—while reducing maintenance requirements and carbon emissions. With over 3 million operating hours globally, these turbines offer a proven solution for energy producers and consumers in Vietnam looking to lower electricity costs without compromising reliability or sustainability.
With the 9HA.02 gas turbine fleet, you can benefit from higher combined-cycle efficiency:
Flexible long-term power
Grid firming, also known as capacity or renewable firming, involves adding reliable energy resources to renewable power plants to help ensure stable power. Flexible power technology—like aeroderivative gas turbines—supports rapid deployment, fast ramp-up and ramp-down, and smooth variable load balancing, making it integrate well with renewables, an essential capability for Vietnam’s power network.
Born from aviation technology, GE Vernova’s aeroderivative portfolio can be used in a wide variety of applications, including utility generation, district heating, mobile power, fast power, and of course, grid stability. These turbines are well-suited for captive power applications such as combined heat and power (CHP) or cogeneration, providing efficient, on-site electricity and thermal energy for industrial facilities and data centers.
The LM2500XPRESS can run on 35% hydrogen, and when an SCR is added to the unit to reduce emissions even further, NOx can be reduced to 2.5 ppm and CO to 4ppm.
The LM6000VELOX* solution offers 99%+ reliability and 98% availability. It can start up in 5 minutes, and its dual-fuel capabilities provides fuel flexibility and helps customers meet emissions limits.
A leader in gas turbine technology
Local presence
GE Vernova is committed to fueling Vietnam’s growth through development of local talent in high value sectors like engineering, and we work with local SMEs and suppliers. Beyond our focus on gas turbines, our solutions also include plant-wide offerings such as steam turbines, generators and HRSGs.
GE Vernova generates up to 30% of Vietnam’s power
Fleet of 25+ gas turbines
6 GE Vernova locations with over 1K+ employees, including the Dung Quat Heat Recovery Steam Generators (HRSG) facility and Phu My gas turbine reconditioning workshop
Servicing 10+ power plants and other projects
A global shift
Vietnam has come a long way since the severe electricity shortages of the 80s and 90s. With today’s electrification rate of 100%, Vietnam’s power capacity has reached 77,600 MW, first in Southeast Asia. The coal-to-gas transition will be key to enabling the growth of renewables and helping to address the energy trilemma of reliability, affordability, and sustainability.
As the country charts a rapid path to more sustainable energy sources, including renewable energy and gas power at scale, Vietnam will need the flexibility, output, and efficiency of natural gas.As the country charts a rapid path to more sustainable energy sources, including renewable energy and gas power at scale, Vietnam will need the flexibility, output, and efficiency of natural gas.
Learn more
Interested in learning more about how GE Vernova is helping support Vietnam’s growth? Our articles and case studies provide additional information, insights and stories from GE Vernova experts in the region. Stay tuned for more to come!
Featured video
The Jawa Satu power plant provides reliable electricity to 10 million people, powered by GE Vernova’s 9HA.02 turbines. It delivers high efficiency and quick grid response, helping Indonesia move toward its net-zero goals with advanced technology and teamwork.
Webinars
Technical knowledge
Services
With local repair capabilities and the strength of our global expertise, GE Vernova is on of the service providers of choice in Asia, where we have up to 90% in-region self-sufficiency for heavy-duty gas turbines—including the HA—and up to 100% in-region self-sufficiency for on-site modular maintenance for aeroderivative gas turbines.

Contact us

Le Dong Hai
Sales Manager, New Unit - Vietnam
*Trademark of GE Vernova and/or its affiliates.