Calibration Management Deployment
Deploy Calibration Management for the First Time
The following table outlines the steps that you must complete to deploy and configure this module for the first time.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
| Step | Task | Notes |
|---|---|---|
| 1 | Assign Security Users to one or more of the Calibration Management Security Roles. | This step is required. |
| 2 | Define alternate search queries. | This step is required only if you do not want to use the baseline search queries. |
| 3 | Configure default values for Calibration Template and Calibration Event Records by accessing the Calibration Setup Defaults family in Application Settings. | This step is required. |
| 4 | Install the GE Device Service on all of the machines that will connect to devices that will be used with Calibration Management. | This step is required only if you are performing an automated calibration. |
Install the GE Device Service
Before You Begin
Important: You must repeat this procedure on every machine to which a calibrator will be connected.
About This Task
You can download the installer from KBA 000059233.
Procedure
What To Do Next
Configure the GE Device Service
Before You Begin
- You need administrative access to the machine on which you want to configure the service.
- Install the GE Device Service.
Important: You must repeat this procedure on every machine to which a datalogger will be connected.
About This Task
This topic describes how to configure the settings, which is required only if:
- Your APM connection uses HTTPS.
- The default port 2014 is not available.