Reliability Analytics Deployment
Deploy Reliability Analytics for the First Time
The following table outlines the steps that you must complete to deploy and configure this module for the first time.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
| Step | Task | Notes |
|---|---|---|
| 1 | Assign Security Users to one or more Reliability Analytics Security Groups and Roles. | This step is required. |
| 2 | Ensure that the Meridium Simulation Service is installed and running. | If the basic APM system architecture is already installed, the Meridium Simulation Service is automatically installed and run. Note: Reliability Simulation service is required to execute the tasks that take a long time. APM Client (browser) will keep polling the APM Server to check the progress of the such tasks and report the progress to the end user in the background. |
| 3 | Configure ActiveMQ Settings for the Simulation Service. | This step is optional. Default values exist for the concurrency limit, number of retries, number of threads, and the time limit of the Simulation Service. You can change these values as needed. |
Configure ActiveMQ Settings for the Simulation Service
Before You Begin
About This Task
This topic describes how to chance the concurrency limit, number of retries, number of threads, and the time limit of the Simulation Service.