Rounds Pro Deployment
Deploy Rounds Pro for the First Time
The following table outlines the steps that you must complete to deploy and configure this module for the first time.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes |
---|---|---|
1 | Review the data model to determine which relationship definitions you will need to modify to include your custom Equipment and Functional Location families. Modify any relationship definitions as needed via Configuration Manager. | This step is required only if you have asset data in families outside of the baseline Equipment and Functional Location families. |
2 | Assign Security Users to the following Rounds Pro
Security Groups:
| This step is required. |
3 | Install the Rounds Pro mobile application on the mobile device that you plan to use for data collection. | This step is required only if you will use a mobile device for data collection. For information on installation of Rounds Pro on mobile devices, refer to the Rounds Pro Mobile documentation. |
4 | Set the local time zone on the mobile device that you will use for data collection, typically the user time zone. | This step is required only if you will use a mobile device for data collection. |