Generation Availability Analysis Wind Deployment
Deploy GAA Wind for the First Time
The following table outlines the steps that you must complete to deploy and configure this module for the first time.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Before you begin completing these tasks, review the system requirements for this module to identify the supported features for this module in APM.
Step | Task | Notes |
---|---|---|
1 | Review the GAA Wind data model to determine which relationship definitions you will need to modify to include your custom equipment and location families. Via Configuration Manager, modify the relationship definitions as needed. | This step is required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families. |
2 | Assign Security Users to one or more of the GAA Wind Security Groups and Roles. | This step is required. |
3 | Specify additional system code tables for the GAA Wind families. | By default, APM provides a set of system code tables for the GAA Wind families. You can modify these default system code tables or add new system code tables. |
4 | Configure the GAA Wind Report Configuration records. | This step is required. |
5 | Using the GAA Wind Asset Hierarchy Data Loader, create the following records in the GAA Wind Asset Hierarchy:
| This step is required. |
6 | Using the GAA Wind Sub Group Capacity Data Loader, create the GAA Wind Sub Group Capacity record. | This step is required. |