Management of Change Deployment

Deploy MoC for the First Time

StepTaskNotes
1 Assign Security Users to one or more of the MOC Security Roles.This step is required.
2 Modify the MI_MOC_ANS_OPT System Code Table.This step is required only if you want to add or modify the values that appear in the Answer field when you create a Question or modify Answer Options in a Question.
3 Modify the MI_Change_Project_Type System Code Table.This step is required only if you want to add or modify the values that appear in the Change Type field, on the MI MOC Change Project datasheet.