Analytic Instance Field Descriptions
Add Analytic Instance Field Descriptions
This topic describes the fields that can be viewed in the Add Analytic window.
Field | Purpose |
---|---|
ANALYTIC NAME | By default, the analytic instance is given the same name as the parent asset. You can modify this name, but it must be unique. |
ANALYTIC TEMPLATE | Select the Analytic Template that must be used from the drop-down list box. |
ANALYTIC TEMPLATE VERSION | Based on the template that is selected the template version appears. |
COLLECTION TYPE | Select one of the following collection types from the drop-down list:
Note: By default, the Collection Type is set to Sample and Hold. However, you can modify the default setting. |
COLLECTION INTERVAL | Set the collection interval in minutes or seconds. Note: By default, the Collection Interval is set based on the configuration of the selected template. However, you can modify the default setting. |