Overview
About Configuring SmartSignal in APM for the First Time
To use SmartSignal with APM, you must have Tenant Admin permissions, and the following functions must be configured:
- If you are using the SmartSignal Mapping application to create or associate an APM asset with a SmartSignal analytic, add and configure the SmartSignal host.
- Configure the SmartSignal tenant.
- Associate the SmartSignal tenant with a host.
- Map SmartSignal analytics to APM assets for the tenant.
- Configure the Sensor Health Monitoring parameters.