Mapping to GED IMS Installation
The topics in this section explain how to configure a hybrid SmartSignal solution that uses both and SmartSignal Classic. This hybrid configuration is not applicable to most users.
About Mappings
You can use the SmartSignal Mappings application to configure and maintain relationships between SmartSignal analytics and APM assets.
The Input Excel File
To map assets, you must first upload an Input Excel File. The input file should contain the following columns and content:
Column Name | Description |
---|---|
APM Asset SourceKey | Name of the APM asset. |
APM Asset Path | The APM hierarchy. Do not include the root node or the asset node in the path. If there are multiple nodes, the delimiter should be > . |
SmartSignal Asset Name | The asset name in the SmartSignal Classic Asset Center. |
SmartSignal Asset Path | Asset hierarchy in the SmartSignal Classic Asset Center. Do not include the root node or the asset node in the path. If there are multiple nodes, the delimiter should be > . |
Host Name | The configured SmartSignal host name in the SmartSignal Global Host Management page. |
Collection Type | Specifies how frequently observations should be processed for this asset. The valid values are:
See the Modify Settings for an Analytic Instance topic for descriptions of each of these data collection type. |
Mappings Procedures
Once you have uploaded an asset input file, you can:
- Import SmartSignal Classic Assets into APM using a transfer file.Note: In APM, SmartSignal Classic assets become analytic instances.
- Associate an APM asset with a SmartSignal analytic.
- Unassociate an APM asset from a SmartSignal analytic.
Access Current Mappings for SmartSignal
In the SmartSignal Mappings application, you can access all of the asset mappings between SmartSignal analytics and APM assets for a tenant.
Procedure
Associate or Unassociate an APM Asset with a SmartSignal Analytic
You can associate or unassociate an APM asset with a SmartSignal analytic using the SmartSignal Mappings page.
Before You Begin
- Both the APM asset and the SmartSignal analytic must exist at the paths provided in the Input Excel File, and all columns in the spreadsheet must be specified.
- You must have selected an input file and validated its contents, such that the SmartSignal analytics appear in the Validate/Action Results table.
A single existing APM asset can be associated with multiple existing SmartSignal analytics. To associate with multiple SmartSignal analytics, you need to do the following:
- In the row containing the first existing SmartSignal asset that you want to associate with the APM asset, use the Associate button if the APM asset already exists. If it doesn't exist yet, use the Create button first.
- For the remaining SmartSignal assets, specify the same APM Asset SourceKey and Path as the first SmartSignal asset and use the Associate button.
About This Task
SmartSignal analytics can only be associated with one APM asset at a time. The last associated action will take precedence. For example, if you have the following spreadsheet and select Associate, SmartSignal asset_1 will be associated with apm_asset_A, and not apm_asset_1.
A | B | C | D | |
---|---|---|---|---|
1 | APM Asset SourceKey | APM Asset Path | SmartSignal Asset Name | Smartsignal Asset Path |
2 | apm_asset_1 | node1>node2>node3 | asset_1 | node1|node2 |
3 | apm_asset_A | nodeA>nodeB | asset_1 | node1|node2 |