Template Tag Field Descriptions
Input Tag and Output Tag Field Descriptions
This topic describes the fields that can be viewed in the Input Tag and Output Tag grid.
Column | Description |
---|---|
Actions | In this column, you can select ![]() ![]() If the tag is configured to generate a calculated value, |
Name | The name of the tag. |
Calculated Estimate | Estimate generated by a user defined expression rather than the reference data selection algorithm. |
Description | The description of the tag. |
Actual High | Thresholds used in rules to determine whether data is outside of expected limits. |
Actual Low | |
Adaptation High | Upper and lower thresholds used to determine the range of data that can be adapted into models from runtime using the auto-adaptation algorithms. |
Adaptation Low | |
Tag ID | Automatically generated unique ID for the tag. This value cannot be modified. |
Measurement Units | The units of measure for the source data of the tag, such as degrees (C) or percentage (%). This is used only as an identifying label and is displayed on the y-axis when the tag is used in model training data charts. |
Standard Units | The units of measurement for the source data for the tag. |
Data Type | The data format of the tag. The options are Float, Integer, Boolean, String, or Date. The data type cannot be changed once a tag is added and the analytic template is saved. |
Tag Type | If the tag is configured to generate a calculated value, ![]() ![]() |
Decimal Scale | The number of decimal places included in the tag readings. This value is inherited from templates imported from Classic SmartSignal Blueprint Center. It is not used in APM and cannot be modified. |
Step High Threshold | Thresholds used for step-change rules. |
Step Low Threshold | |
Notes | Notes about the tag. |
Chart Y Min | Chart Y Min and Max values override default chart automatic scaling on the y-axis. In other words, by default, analysis charts are automatically scaled on the y-axis based on tag reading values. For example, if you have a tag with reading values that range from 10 through 30, the bottom of the y-axis in the chart has a value of 10, and the top of the y-axis has a value of 30. If you prefer to see a chart that starts at 0 and ends at 50 in the y-axis, you can enter 0 in the Chart Y Min column and 50 in the Chart Y Max column. Note: If you imported an analytic template from a SmartSignal Classic blueprint, if that blueprint had Chart Y Min and Max values, those values are maintained in APM.
|
Chart Y Max |
Output Tag Field Descriptions
This topic describes the fields that can be viewed in the Output Tag grid.
Column | Description |
---|---|
Actions | In this column, you can select ![]() ![]() If the tag is configured to generate a calculated value, |
Name | The name of the tag. |
Calculated Estimate | Estimate generated by a user defined expression rather than the reference data selection algorithm. |
Description | The description of the tag. |
Actual High | Threshold used in rules to determine whether data is outside of expected limits. |
Actual Low | Threshold used in rules to determine whether data is outside of expected limits. |
Adaptation High | Upper threshold used to determine the range of data that can be adapted into models from runtime using the auto-adaptation algorithms. |
Adaptation Low | Lower threshold used to determine the range of data that can be adapted into models from runtime using the auto-adaptation algorithms. |
Tag ID | Automatically generated unique ID for the tag. This value cannot be modified. |
Measurement Units | The units of measure for the source data of the tag, such as degrees (C) or percentage (%). This is used only as an identifying label and is displayed on the y-axis when the tag is used in model training data charts. |
Standard Units | The units of measurement for the source data for the tag. |
Data Type | The data format of the tag. The options are Float, Integer, Boolean, String, or Date. The data type cannot be changed once a tag is added and the analytic template is saved. |
Tag Type | If the tag is configured to generate a calculated value, ![]() ![]() |
Decimal Scale | The number of decimal places included in the tag readings. This value is inherited from templates imported from Classic SmartSignal Blueprint Center. It is not used in APM and cannot be modified. |
Step High Threshold | Threshold used for step-change rules. |
Step Low Threshold | |
Notes | Notes about the tag. |
Constant Tag Field Descriptions
This topic describes the fields that can be viewed in the Constant Tag grid.
Column | Description |
---|---|
Actions | In this column, you can select ![]() |
Name | The name of the tag. |
Description | The description of the tag. |
Data Type | The data format for the tag. The options are Float, Integer, Boolean, String, or Date. Once a tag is added and the analytic template is saved, you cannot modify the data type. |
Default Value | The default value for the tag. Note: For constant tags with a type of Date, no default value can be selected. |
Notes | Notes about the tag. |
Column | Description |
---|---|
Actions | In this column, you can select ![]() |
Name | The name of the tag. |
Mode | The mode with which the tag is associated. |
Model | The model with which the tag is associated. |
Description | The description of the tag. |
Data Type | The data format for the tag. The options are Float, Integer, Boolean, String, or Date. Once a tag is added and the analytic template is saved, you cannot modify the data type. |
Default Value | The default value for the tag. Note: For constant tags with a type of Date, no default value can be selected. |
Notes | Notes about the tag. |
Modes Field Descriptions
This topic describes the fields that can be viewed in the Modes grid.
Field | Purpose |
---|---|
Actions | In this column, you can select ![]() |
Name | The name for the mode analytic template. |
Description | The description for this mode analytic template. |
Expression | The expression used to define the mode condition. |
Is Valid | Boolean value used to determine the validity of the expression. |
Notes | The notes for this mode analytic template. |
Models Field Descriptions
This topic describes the fields that can be viewed in the Models grid.
Field | Purpose |
---|---|
Actions | In this column, you can select ![]() |
Display Name | The name of the model analytic template. |
Mode | The mode with which the tag is associated. |
Description | Description of the model analytic template. |
Estimate Generator | A reference data selection algorithm used to generate estimated values. There are two types of estimate generators:
|
Similarity Operator | One of the following algorithms used for modeling:
|
Enable VSG | Specifies whether or not virtual signal generation is enabled. If NaNs and/or outliers are encountered and the number of tags containing bad data is below the Maximum % of Bad Tags threshold, the system will fill in the missing or bad data for modeled tags with virtual signal data. |
Max Percentage of Bad Tags | The percentage threshold above which the system inhibits virtual signal generation. |
Variance Scale Factor | A multiplier for the standard deviation of normal residual signals. |
Residual Smoothing - Smoothing Algorithm |
|
Residual Smoothing - Window Size | The total window (the number of data points or persistence) to use for smoothing. |
Residual Smoothing - Spline | A number between 0 and 1, where the value 0 causes the greatest smoothing and a value of 1 results in no smoothing (the output values equal the input values). A typical default value is 0.1. |
State Matrix Creation - Down Sample Algorithm | One of the following algorithms that is used when creating the state matrix:
|
Maximum Vectors | The maximum number of vectors to include in the state matrix. This option works with models that have auto adaptation. If the maximum vectors are larger than the target vectors, it will increase the size of the state matrix. For example, if the target vectors is set to 25 and the maximum vectors is set to 50, the first 25 times auto adaptation occurs, the state matrix will become larger, then it will stop increasing at 50. If the maximum vectors is smaller than the target vectors, this field will have no effect. |
State Matrix Creation - Target Vectors | The number of vectors that will be targeted when the state matrix is created. Used when Vector Ordering is specified in the Downsample Algorithm box. |
VBM - Fixed Size LocalD |
|
Similarity Percentile | Threshold used to determine whether or not vectors are different enough from each other to both be considered for the VBM state matrix. |
Redundancy Check Time | Specifies when redundancy checks are to be executed (e.g., during runtime or setup of the model). |
Reference Data Splits | The number of sections to which the MinMax algorithm should be applied. Used when Min Max Split is specified in the Downsample Algorithm box. |
Notes | Notes about the model analytic template. |
Created Date | Date the model analytic template was created. |
Last Changed Date | Date the model analytic template was last modified. |
Model Tags Field Descriptions
This topic describes the fields that can be viewed in the Model Tags grid.
Column | Description |
---|---|
Actions | In this column, you can select ![]() |
Name | The name of the tag. |
Is In Model | If selected, this analytic template tag will be included as part of the model blueprint. The collection of model-specific settings and data for this tag are collectively referred to as a model tag. |
Mode | The mode with which the tag is associated. |
Model | The model with which the tag is associated. |
Alarm Type | Defines the algorithm used to trigger residual indications.
|
Is Independent | Inferential models use an observation of measured signal values to generate one or more estimated signal values not present in the observation of measured signal values. When using this method, this field indicates whether the independent variables should represent all of the drivers for the dependent output variables. |
Is Driver | Any tags with this selected will be looked at to determine if a new operating state is occurring to trigger auto adaptation. At least one tag must be checked to enable auto-adaptation. |
Residual Variance | Used to set a custom value of residual variance for use by the SPRT algorithm. If not set, each Asset will use the variance if the residual across its training data. Do not change this setting without fully understanding what it does. |
Negative Outlier Threshold | Threshold used for outlier rules. |
Positive Outlier Threshold | Threshold used for outlier rules. |
Negative Residual Threshold | The maximum absolute value allowed for a negative residual (i.e., when the estimate is below the actual for a signal). See details in the Alarm Type column. |
Positive Residual Threshold | The maximum absolute value allowed for a positive residual (i.e., when the estimate is above the actual for a signal). See details in the Alarm Type column. |
Negative SPRT Sensitivity | The negative values for the sensitivity of the SPRT. This value is multiplied by the standard deviation of the residual, which in turn defines the amount of negative change in the residual mean that must occur to constitute an alarm. |
Positive SPRT Sensitivity | The positive values for the sensitivity of the SPRT. This value is multiplied by the standard deviation of the residual, which in turn defines the amount of positive change in the residual mean that must occur to constitute an alarm. |
Model Tag Display Name | The display name of the tag. |
Data Type | The data format for the tag. The options are Float, Integer, Boolean, String, or Date. |
Tag Type | The type of tag (i.e., Input, Output, or Constant). |
Description | The description of the tag. |
Filter High | The upper filtering threshold. This field sets the upper threshold value for filtering of tag signals to remove data outside the normal operating range. Any tag data greater than this value is considered an outlier. Outliers will be filtered out of training data. |
Filter Low | The lower filtering threshold. This field sets the lower threshold value for filtering of tag signals to remove data outside the normal operating range. Any tag data less than this value is considered an outlier. Outliers will be filtered out of training data. |
Flat Line Number | If the data for this tag remains at the same level for more than this number of data points, the data will be considered to be flat lined, and will be filtered out of training data. |
Spike Sensitivity | The sensitivity of the spike detection algorithm used to detect spikes in tag signals. A higher value will detect more spikes, but may also generate false positives. Spike data will be filtered out of training data. Do not change this setting without fully understanding what it does. |
Notes | The notes for the tag. |
Diagnostic Rules Field Descriptions
This topic describes the fields that can be viewed in the Diagnostic Rules grid.
Field | Purpose |
---|---|
Actions | In this column, you can select ![]() |
Name | The name for the diagnostic rule. |
Expression | The expression used to define the mode condition. |
Is Valid | Boolean value used to determine the validity of the expression. |
Startup Suppression Poll Cycles | Specifies the number of poll cycles the rule will be suppressed (that is, not evaluated) after the asset enters a new mode. |
Active | Boolean values that determines whether the tag is active or inactive. |
Description | The description for the diagnostic rule. |
Notes | The notes for the diagnostic rule. |
Tag Rules Field Descriptions
This topic describes the fields that can be viewed in the Tag Rules grid.
Field | Purpose |
---|---|
Actions | In this column, you can select ![]() |
Display Name | Displays the name of the rule. A green check mark displayed next to the name field indicates that the item is ready to be used. A yellow triangle indicates that the rule is not ready to be used. Hover over the yellow triangle to see which information is missing from the rule. |
Description | A description for this rule. |
Mnemonic | Abbreviation used to identify the rule to assist with references in diagnostics rules. |
Suppression Poll Cycle | Specifies the number of poll cycles the rule will be suppressed (that is, not evaluated) after the asset enters a new mode. |
Priority | The priority of the rule; affects display of advisories in the application. |
Message | Configures the message that will appear for the advisory. There are four options that can be displayed in the message: Source Tag, Description, Alias, and Asset. |
Expression | The expression used to define the mode condition. |
Notes | Notes for this rule. |
Input Tag UOM
This topic lists the UOM names that are currently supported by the SmartSignal Input Tag UOM conversion feature.
Category | Name | Description | Alias name in APM UOM |
Pressure | PSIG | Pound-force per square inch gauge | psi g, psig, PSIG |
PSIA | Pounds-force per square inch absolute | psi a, psia, psi, PSIA | |
inHg | Inches of mercury | in.Hg, inHgA, inHg a, inHg | |
mmHg | Millimeters of mercury | mm.Hg a, mmHg, | |
inH2O | Inches of water | in.H2O a, inH2O | |
ftH2O | Feet of water | ft.H2O a,ftH2O | |
Bar | Units of pressure | bar,bar a, Bar, BAR | |
Pa | Pascal | Pa | |
KPa | Kilopascals | KPa | |
Torr | Units of pressure | Torr | |
Atm | Atmospheres | atm | |
BarG | Bars gauge | barg, bar g, bar(g), BarG | |
mmH2O | Millimeters of water | mm.H2O, mm.H2O a, mmH2O | |
mBar | Millibar | mBar | |
MPa | Megapascal | MPa | |
hPa | Hectopascal | hPa, HPA | |
daPa | Dekapascal | daPa | |
dPa | Decipascal | dPa | |
cPa | Centipascal | cPa | |
milliPa = 49, | Millipascal | mPa, milliPa | |
μPa | Micropascal | uPa | |
KilogramsPerSquareCentimeterAbsolute | kg/cm^2 a | KilogramsPerSquareCentimeterAbsolute, kg/cm2 a | |
KilogramsPerSquareCentimeterGauge | kg/cm^2 g | KilogramsPerSquareCentimeterGauge, kg/cm2 g | |
inHgG | Inches of mercury Gauge | inHgG, in.Hg g | |
mmHgG | Millimeters of mercury Gauge | mmHgG , mm.Hg g | |
inH2OG | Inches of water Gauge | in.H2O g, inH2OG | |
ftH2OG | Feet of water Gauge | ft.H2O g, ftH2OG | |
mmH2OG | Millimeters of water Gauge | mm.H2O g, mmH2OG | |
mBarG | Millibar Gauge | mBarG, mBarg, mBar g,mBarG | |
Temperature | Celsius | Celsius | Celsius, Deg C, deg C, DEG C |
Fahrenheit | Fahrenheit | Fahrenheit, Deg F, deg F, DEG F | |
Kelvin | Kelvin | Kelvin | |
Rankine | Rankine | Rankine | |
Frequency | RPM | Revolutions per minute | rpm, RPM |
CPS | Cycles per second | cycles/sec, cycles/s, CPS | |
CPM | Cycles per minute | cycles/min, CPM | |
Speed | FPM | Feet per minute | ft/min, FPM |
MPM | Meters per minute | m/min, MPM | |
IPS | Inches per second | in/sec, in/s, IPS | |
MetersPerSecond | m/sec | m/sec, m/s, MetersPerSecond | |
MillimetersPerSecond | mm/sec | mm/sec, mm/s, MillimetersPerSecond | |
MicrometersPerSecond | μm/sec | um/sec, um/s, MicrometersPerSecond | |
FeetPerSecond | ft/sec | ft/sec, ft/s, FeetPerSecond | |
Hertz | Hz | Hz, Hertz | |
FlowRateVolume | GPM | Gallons per minute | gal/min, GPM |
GPH | Gallons Per Hour | gal/hr, GPH | |
CFM | Cubic feet per minute | ft3/min, CFM | |
m3PerHour | Cubic meters per hour | m3/hr, m3PerHour | |
LPS | Liters per second | liter/sec, liter/s, LPS | |
LBMPerHour | Pounds mass per hour | lbm/hr, LBMPerHour, lb/hr | |
kLBMPerHour | Kilo-pounds mass per hour | klbm/hr, kLBMPerHour | |
kgPerHour | Kilograms per hour | kg/hr, kgPerHour | |
kgPerSecond | Kilograms per second | kg/sec, kg/s, kgPerSecond | |
CFS | Cubic feet per second | ft3/sec, ft3/s, CFS | |
CFH | Cubic feet per hour | ft3/hr, CFH | |
CFD | Cubic feet per day | ft3/day, CFD | |
kCFM | Thousands of Cubic feet per minute | k(ft3)/min, kCFM | |
kCFS | Thousands of Cubic feet per second | k(ft3)/sec, kCFS | |
kCFH | Thousands of Cubic feet per hour | k(ft3)/hr , kCFH | |
kCFD | Thousands of Cubic feet per day | k(ft3)/day, kCFD | |
MCFM | Millions of Cubic feet per minute | M(ft3)/min, MCFM | |
MCFS | Millions of Cubic feet per second | M(ft3)/sec, M(ft3)/s, MCFS | |
MCFH | Millions of Cubic feet per hour | M(ft3)/hr, MCFH | |
MCFD | Millions of Cubic feet per day | M(ft3)/day, MCFD | |
GPS | Gallons per second | gal/sec, gal/s, GPS | |
GPD | Gallons per day | gal/day, GPD | |
m3PerSecond | Cubic meters per second | m3/sec, m3/s, m3PerSecond | |
m3PerMinute | Cubic meters per minute | m3/min, m3PerMinute | |
m3PerDay | Cubic meters per day | m3/day, m3PerDay | |
LPM | Liters per minute | liter/min, LPM | |
LPH | Liters per hour | liter/hr , LPH | |
LPD | Liters per day | liter/day,LPD | |
ccPerSecond | Cubic centimeters per second | cm3/sec, cm3/s, ccPerSecond | |
ccPerMinute | Cubic centimeters per minute | cm3/min, ccPerMinute | |
ccPerHour | Cubic centimeters per hour | cm3/hr, ccPerDay | |
ccPerDay | Cubic centimeters per day | cm3/day, ccPerDay | |
FlowRateVolume | in3PerSecond | Cubic inches per second | in3/sec, in3/s, in3PerSecond |
in3PerMinute | Cubic inches per minute | in3/min, in3PerMinute | |
in3PerHour | Cubic inches per hour | in3/hr, in3PerHour | |
in3PerDay | Cubic inches per day | in3/day, in3PerDay | |
FlowRateVolume | BBS | Barrels (oil) per second | bbl/sec, bbl/s, BBS |
BBM | Barrels (oils) per minute | bbl/min, BBM | |
BBH | Barrels (oils) per hour | bbl/hr, BBH | |
BBD | Barrels (oils) per day | bbl/day, BBD | |
kBBS | Thousands of Barrels (oil) per second | kbbl/sec, kbbl/s, kBBS | |
kBBM | Thousands of Barrels (oils) per minute | kbbl/min, kBBM | |
kBBH | Thousands of Barrels (oils) per hour | kbbl/hr, kBBH | |
kBBD | Thousands of Barrels (oils) per day | kbbl/day, kBBD | |
MBBS | Millions of Barrels (oil) per second | Mbbl/sec, Mbbl/s, MBBS | |
MBBM | Millions of Barrels (oils) per minute | Mbbl/min, MBBM | |
MBBH | Millions of Barrels (oils) per hour | Mbbl/hr, MBBH | |
MBBD | Millions of Barrels (oils) per day | Mbbl/day, MBBD | |
LBMPerSecond | Pounds mass per second | lbm/sec, lbm/s, LBMPerSecond, lb/s, lb/sec | |
LBMPerMinute | Pounds mass per minute | lbm/min, LBMPerMinute, lb/min | |
LBMPerDay | Pounds mass per day | lbm/day, LBMPerDay, lb/day | |
kLBMPerSecond | Kilo-pounds mass per second | klbm/sec, klbm/s, kLBMPerSecond | |
kLBMPerMinute | Kilo-pounds mass per minute | klbm/min, kLBMPerMinute | |
kLBMPerDay | Kilo-pounds mass per day | klbm/day, kLBMPerDay | |
MLBMPerHour | Mega-Pounds mass per hour | Mlbm/hr, MLBMPerHour | |
MLBMPerSecond | Mega-Pounds mass per second | Mlbm/sec, Mlbm/s, MLBMPerSecond | |
MLBMPerMinute | Mega-Pounds mass per minute | Mlbm/min, MLBMPerMinute | |
MLBMPerDay | Mega-Pounds mass per day | Mlbm/day, MLBMPerDay | |
kgPerMinute | Kilograms per minute | kg/min, kgPerMinute | |
kgPerDay | Kilograms per day | kg/day, kgPerDay | |
MetricTonPerSecond | Metric Ton per second | Metric Ton/sec, MetricTonPerSecond | |
MetricTonPerMinute | Metric Ton per minute | Metric Ton/min, MetricTonPerMinute | |
MetricTonPerDay | Metric Ton per day | Metric Ton/day, MetricTonPerDay | |
MetricTonPerHour | Metric ton per hour | Metric Ton/hr, MetricTonPerHour | |
FlowRateVolume | ThousandsOfCubicMetersPerSecond | k(m^3)/s | k(m3)/sec, k(m3)/s, ThousandsOfCubicMetersPerSecond |
ThousandsOfCubicMetersPerMinute | k(m^3)/m | k(m3)/min, ThousandsOfCubicMetersPerMinute | |
ThousandsOfCubicMetersPerHour | k(m^3)/h | k(m3)/hr, ThousandsOfCubicMetersPerHour | |
ThousandsOfCubicMetersPerDay | k(m^3)/d | k(m3)/day, ThousandsOfCubicMetersPerDay | |
MillionsOfCubicMetersPerSecond | M(m^3)/s | M(m3)/sec, MillionsOfCubicMetersPerSecond | |
MillionsOfCubicMetersPerMinute | M(m^3)/m | M(m3)/min, MillionsOfCubicMetersPerMinute | |
MillionsOfCubicMetersPerHour | M(m^3)/h | M(m3)/hr, MillionsOfCubicMetersPerHour | |
MillionsOfCubicMetersPerDay | M(m^3)/d | M(m3)/day, MillionsOfCubicMetersPerDay | |
Power | HP | Horsepower (International) | hp, HP |
W | Watts | W | |
MW | Megawatts | MW | |
kW | Kilowatts | kW | |
NmPerSecond | Newton meters per second | N-m/sec, NmPerSecond | |
BTUPerHour | BTU / Hour | btu/hour, BTUPerHour | |
MBTUPerHR | Million BTU / hour | Mbtu/hr, MBTUPerHR | |
Var | Var (varistor) | Var | |
Millivar | mVar | mVar, Millivar | |
Kilovar | kVar | kVar, Kilovar | |
Megavar | MVar | MVar, Megavar | |
Torque | FtLBF | Foot pounds force | ft-lbF, FtLBF |
Nm | Newton meter | N-m, Nm | |
Length | ft | Feet | ft |
In | Inches | in, In | |
m | Meters | m | |
mm | millimeters | mm | |
cm | centimeters | cm, | |
mils | a mil = a thousandth of an inch | mils , MILS | |
μm | Micrometers | um | |
Mass | Pounds | lbm | lbm, Pounds |
Kilopounds | klbm | klbm, Kilopounds | |
Kilograms | kg | kg, Kilograms | |
ElectricCurrent | Amps | A | A, Amps |
Milliamps | mA | mA, Milliamps | |
Kiloamps | kA | kA, Kiloamps | |
ElectricPotential | Volts | V | V, Volts |
Millivolts | mV | mv, Millivolts | |
Kilovolts | kV | kV, Kilovolts | |
Time | Seconds | seconds | seconds |
Minutes | minutes | minutes | |
Hours | hours | hours | |
Days | days | days | |
Years | years | years | |
StmSpecificEnthalpy | BTUPerLbm | Stem Table Function, Specific Enthalpy British Unit, Btu/Lbm | btu/lbm, BTUPerLbm |
JPerkg | Stem Table Function, Specific Enthalpy SI Unit, J/kg | not found ????? | |
kJPerkg | Stem Table Function, Specific Enthalpy SI Reference unit, kJ/kg | kJ/kg, kJPerkg | |
BTUPerLbmF | Stem Table Function, Specific Entropy British unit, BTU/Lbm/F | btu/lbmf, BTUPerLbmF | |
kJPerkgK | Stem Table Function, Specific Entropy SI unit, kJ/kg/K | kJPerkgK, | |
JPerkgK | Stem Table Function, Specific Entropy SI Reference unit, J/kg/K | j/kgk, JPerkgK | |
StmSpecificVolume | CubicFeetPerLb | Stem Table Function, Specific Volume British unit, Ft^3/Lb | cubicfeet/lb, CubicFeetPerLb |
CubicMeterPerKg | Stem Table Function, Specific Volume SI unit, m^3/kg | cubicmeter/kg, CubicMeterPerKg | |
StmThermoConductivity | BTUPerHrFtF | Stem Table Function, ThermoConductivity British unit, BTU/hr/ft/F | btu/hrftf, BTUPerHrFtF |
WattPerMeterK | Stem Table Function, ThermoConductivity SI unit, Watt/m/C | watt/meterk, WattPerMeterK | |
StmDynamicViscosity | LbmPerFtHr | Stem Table Function, DynamicViscosity British unit, Lbm/ft/hr | lbm/fthr, LbmPerFtHr |
Centipoise | Stem Table Function, DynamicViscosity SI unit, Centipoise, 1e-3 kg/m/s | centipoise, Centipoise | |
PaSec | Stem Table Function, DynamicViscosity SI Formal unit, Poise (analog to Pa * s), kg/m/s | pasec, PaSec |