Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataStore Class / IsDefault Property


IsDefault Property
Whether the data store is marked as default store (used as default data store for tags adds, and archive related operations)
Syntax
Public Property IsDefault As System.Boolean
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also