Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataStore Class / State Property


State Property
The state of the data store.
Syntax
Public Property State As DataStore.DataStoreState
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also