Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianFault Class / Status Property


Status Property (HistorianFault)
An error status underlying the fault.
Syntax
Public Property Status As Status
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also