Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianFault Class / HistorianFault Constructor / HistorianFault Constructor(Status)
A status value.


HistorianFault Constructor(Status)
Alternative constructor accepting a specific error status.
Syntax
Public Function New( _
   ByVal status As Status _
)

Parameters

status
A status value.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also