Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IAlarms Interface / Delete Method


Delete Method (IAlarms)
This provides the functionality to delete or purge Alarms and event from the Alarms and Events database.
Syntax
Sub Delete( _
   ByVal backupFileName As System.String, _
   ByVal shouldZipAlarms As System.Boolean, _
   ByVal startTime As System.Date, _
   ByVal endTime As System.Date _
) 

Parameters

backupFileName
shouldZipAlarms
startTime
endTime
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also