Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IAlarms Interface / Restore Method


Restore Method
This provides the functionality to restore alarms and events from a bacup file.
Syntax
Sub Restore( _
   ByVal restoreFileName As System.String _
) 

Parameters

restoreFileName
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also