Gauge Bar
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets |
Gauge Bar Properties
Field Name | Description |
---|---|
Input Value | See Set Up Data Binding for Widgets When manually configuring the data source, make sure that the first output field is always set as a 'value' and the second output field as a 'string.' This structure is essential for the proper functioning of the widget. For example, in a Bar Gauge, you might set the first output field to 75 (value) and the second output field to Temperature (string). |
Minimum Value | Sets the minimum scale value. |
Maximum Value | Sets the maximum scale value. |
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. |
Palette | Provides a list of built-in themes that help apply consistent color
schemes across widgets, allowing you to quickly customize their look. Each
theme comes with its own set of unique colors, defining the visual appearance
of the widget.
Note: This feature is currently available only for a
select few widgets. |
Show Legend | Select the check box to display a legend on the Bar Gauge. After
enabling the legend, you can choose how the information is displayed:
|
Angles |
|
Show Label | Select the check box to display a label name, if provided. |
Show Animation | Select the check box to display animation. |
Hidden | Select this check box if you want to hide the widget.
To show the hidden widget in Operations Hub new
layout, go to Page Visuals
and under Action column,
select ![]() |
Bar Gauge at Runtime