Gauge Circular
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets |
Gauge Circular Properties
Field Name | Description |
---|---|
Input Value | See Set Up Data Binding for Widgets |
Minimum Value | Sets the minimum scale value. |
Maximum Value | Sets the maximum scale value. |
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. |
Advanced Settings |
|
Angles | Defines the range of the gauge's scale.
|
Range(s) | You can specify one or more ranges to display in different colors.
|
Hidden | Select this check box if you want to hide the widget.
To show the hidden widget in Operations Hub new
layout, go to Page Visuals
and under Action column,
select ![]() |
Circular Gauge at Runtime