Gauge Linear

Operations Hub New Layout Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub.
Operations Hub Classic Layout Refer to About Widgets

Gauge Linear Properties

Field Name Description
Input Value See Set Up Data Binding for Widgets
Minimum Value Sets the minimum scale value.
Maximum Value Sets the maximum scale value.
Use Raw Format Select the check box to display numbers in raw format.

For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off.

Number of decimals This option appears if you do not want to display numbers in raw format.

In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number.

Advanced Settings
  • Choose an orientation for the linear gauge:
    • Horizontal: Data values appear on a horizontal scale.
    • Vertical: Data values appear on a vertical scale.
  • Select the Show Range Bar check box to dynamically show the highest and lowest value on the linear gauge scale.
  • Select a default color for the range bar.
Range(s) You can specify one or more ranges to to display in a different color.
  1. Select +Add Item.
  2. Specify a value range by entering values for Start of Range and End of Range.
  3. Select a unique color for the specific range.
Hidden Select this check box if you want to hide the widget. To show the hidden widget in Operations Hub new layout, go to Page Visuals and under Action column, select for the hidden widget. See Page Visuals Tab.

Linear Gauge at Runtime

Example of a horizontal orientation:

Example of a vertical orientation: