Text Display
Use this plug-in to add display-only text in your application.
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets |
Text Properties
Field Name | Description |
---|---|
Label | Provide the input data source to receive label names for the text plugin. |
Input Value | See Set Up Data Binding for Widgets |
Align | Choose from:
|
Line Height | Sets the spacing between lines of text. Increasing the line height creates more space between the lines. This can make the text more readable, which is particularly helpful for longer text. Decreasing the line height reduces the line space, which might help in compact layouts where space is limited. |
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of Decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. The decimals will apply to Input Value, Minimum Value, and Maximum Value properties. |
Label Styling | Formats the label: Font Family, Font Size, and Font Color formats the text. |
Hidden | Select this check box if you want to hide the widget.
To show the hidden widget in Operations Hub new
layout, go to Page Visuals
and under Action column,
select ![]() |