Proficy MDC Workflow

Proficy MDC processes data using the following workflow:
  1. Ingestion: Data is ingested from the Plant Applications database to a cloud server. After ingestion, Proficy MDC uses data models to create relationships between the various tables in the cloud server.
  2. Validation: Data is validated to ensure that the record count and data accuracy are intact.
  3. Data Lakes: Data is copied to a data lake so that it can be integrated with data from other systems.