About Custom Calls

Custom Calls allow you to configure and integrate an external service as a PRE or a POST call with an action performed in the integrated application. This configuration is action-specific, not application-specific. For example, for any action (Clock on/off, BOM Item Consumption/ Selection, or Complete), if there is any PRE/POST call configuration created, the expected behavior is same in the Unit Operations, Work Queue, and Process Order applications.

The Custom Calls tab allows you to manage the following actions and their respective tasks:
Actions Perform Tasks
Activity Complete Mark an activity as completed once all associated tasks are finished.
Activity Perform Execute assigned activities by following specified workflows.
Activity Release Release an activity for execution or make it available for the next task in the workflow.
Activity Skip Skip an activity in the workflow when required.
BOM Item Consumption Track and manage the consumption of BOM items during the execution of operation.
BOM Item Selection Select specific BOM items required for a task or process.
BOM Release Approve and release a BOM for use in the production process.
Clock Off Clock off from an operation after completion.
Clock On Clock on to start an operation.
Complete Mark an overall workflow, process, or task as complete.
Manual Skip Manually skip an activity or step in the workflow when necessary.
Receiver Lot Accept Accept a lot of materials or items received during the production process.
Receiver Save Lot Details Save detailed information about the received lot.
Record Quantity Make a record of the quantities produced, consumed, or received during a process.
Release Route Approve and release a route for use in the production process.
Submit Defect Report a non-conformance and submit details of any defects identified during production.
Submit Disposition Provide a resolution or disposition for reported defects.
Validate Operation Confirm that an operation has been executed correctly and meets requirements.
Work Order Complete Mark a work order as completed once all associated activities are finished.
Following are the additional tasks that you can perform:
Note:

When you select Submit to create a non-conformance, you can execute a PRE or POST call from an external service in response to the Submit Defect action. You can configure the custom calls for the Submit Defect action in the Configuration application. The custom call will be executed, and a Pass/Fail message will be displayed accordingly.