About Custom Tab
Custom tabs are useful to load external third-party web applications. Using Configuration, you
can add and configure (the information that will be displayed) custom tabs to the
following applications:
- Activities
- Unit Operations
- Work Queue
- Work Order Manager
- Process Orders
- Receiving Inspection
- Genealogy
Note:
The external application URL must be Cross-Origin Resource Sharing (CORS)-enabled
so that specified input parameters or custom properties can be transferred from the
integrated application to the external application.
In this page, you can perform the following tasks:
- Create a new custom tab and associate it to
any of the applications:
- Activities
- Unit Operations
- Work Queue
- Work Order Manager
- Process Orders
- Receiving Inspection
- Genealogy
- Adding input parameters to custom tab URLs.
- Modify a custom tab.
- Delete a custom tab.