Add Input Parameters to Custom Tab URLs
Procedure
- In the CUSTOM TAB page, under Tab Configuration, select Add another input parameter.The PARAMETER box appears.
- Select an input parameter from the PARAMETER box.Note:The input parameters are a list of all property definitions including definitions under the MaterialLot and Material property groups. However, the Configuration application does not support the property definitions within the MaterialLot Import and Material Import property groups even though they are listed.
- Enter the alias name in the ALIAS text box based on the selected input parameter. Note:The alias name is the external application’s input parameter. It is mapped to the internal application’s input parameter to read values.