Add a User-Defined Event

Procedure

  1. Log in to Plant Applications Web Client.
  2. In the application navigation menu, select .
    The Open page appears.
  3. Select , and then select User Defined Event.
    The Add User Defined Event window appears, displaying a list of user-defined autolog sheets accessible to you as configured in Plant Applications Administrator.
  4. In the Choose activity section, select an activity to create a user-defined event on the selected activity.
  5. In the Add Event Details section, in the EVENT NUMBER box, enter a unique event number.
  6. In the DURATION box, select a start and end time for the event.
  7. Optional: Specify values for the following properties: STATUS, APPLIED PRODUCT, and COMMENT.
    Note:
    When the status of a user-defined event associated with the activity is set to a production status that has the Lock Event Data option enabled, you do not have the privilege to modify the autolog sheet for that event.
  8. In the REASONS box, select a reason to create a user-defined event.
  9. Select Save.

Results

The user-defined event for the selected activity is added and an activity is automatically created for the event. The activity appears in the Open page.