Modify a Non-Conformance

Procedure

  1. Access the non-conformance that you want to modify.
  2. In the row containing one of the defects of the non-conformance, select .
    The Edit Non Conformance window appears.
  3. Provide values as specified in the following table.
    BoxDescription
    SUMMARYEnter the summary of the non-conformance. A value is required.
    NON CONFORMANCE TYPEThis box is disabled and populated with the value Manufacturing Defect.
    DEFECT TYPESelect the type of the defect associated with the non-conformance. A value is required.
    DEFECT REASONSelect Select Reason, specify the hierarchical set of reasons for the non-conformance, and then select Apply.
    Note:
    The reasons that appear in the Select Reasons window are pre-defined in Plant Applications Administrator, and appear based on the value in the NON CONFORMANCE TYPE box. If you want to modify the list of reasons, contact your administrator.
    FULL DESCRIPTIONEnter the full description of the non-conformance.
    ASSIGNEE This field is optional. Select the groups/user(s) to whom you want to assign the defects. You can also deselect the assignees and reassign the defects to other users.
  4. Select Submit.
    The non-conformance is modified.