Access a Non-Conformance
Procedure
- In the Non Conformance page, select Show all Open.A list of all the defects, grouped by the associated non-conformance, appears in the workspace. The following table provides the description of the columns in the table. Click
to select the columns to display in the table.
Column Description STATUS The status of the defect. SERIAL/LOT# The serial/lot number of the defective part. You can select the link in this column to search for all the defects associated with the serial/lot. PLAN The disposition plan created for the defect. You can select the link in this column to search for defects associated with the disposition plan. For a defect in the Submitted state, the value in this column is blank. OP The operation during which the defect was created. MATERIAL The material of the defective part. You can select the link in this column to search for defects associated with the material. MATERIAL FAMILY The material family associated with the defective serial/lot. AFFECTED QUANTITY The quantity of the defective serials/lots for the non-conformance. For a serialized product, the value in this column is always 1. MATERIAL DESC The description of the material of the defective serial/lot. RECEIVER NUMBER The name of the receiver material lot. This field is populated when a defect is created on material lot(s) in the Receiving Inspection app. DISP The method of disposition performed on the defective serial/lot. For a defect in the Submitted status, the value in this column is blank. CTP/REWORK OP The operation until which a defective serial/lot can be processed before disposing the defect. This is applicable only if the disposition method for the defect is Continue-to-Process (CTP). During the operation specified in this column, the defect must be disposed. NC The unique identifier automatically generated by the application when the non-conformance was created. WORK ORDER The name of the discrete work order. DEFECT REASON <number> The hierarchy of reasons identified for the defect. UNIT The name of the equipment or unit. For defects created in discrete apps, the unit is associated with the operation the defect is created on. For defects created in Receiving Inspection, the unit is associated with the material lot it is based on. ACTION REASON <number> The hierarchy of actions identified for the defect. DEFECT MODIFIED BY The last user who modified the defect. DEFECT MODIFIED ON The date and time the defect was last modified. DEFECT ID The unique identifier automatically generated by the application when the non-conformance was created. SUMMARY The brief description of the defect/non-conformance that was entered when the non-conformance was created. ACTIONS The actions you can perform on the serial/lot. Contains the following buttons: : Select this button to dispose the defect. This button is enabled only for a defect in the Submitted status.
: Select this button to modify the non-conformance details. This button is enabled only for a defect in the Submitted status.
: Select this button, and then select Remove from Plan to remove the defect from a disposition plan.
-
If you want to access the defects for a non-conformance, select the link for
the non-conformance. Alternatively, in the Enter a Serial/Lot, NCR,
WO, Plan, Material, Material Family, and Receiver Number box,
enter any of the following details associated with the non-conformance:
- Serial/lot number
- Non-conformance number
- Work order number
- Plan number
- Material
- Material Family
- Receiver Number
The entry is added to the left pane. A list of defects associated with the non-conformance or with the entry that you have entered appears in the workspace in the descending order of the created date or modified date. If you search for a defect using a material or material family, the list of defects are categorized as open and closed. -
When a defect is created against material lot(s) in the Discrete Execution
context, the system records the values for the following fields:
- FOUND AT OP: The operation where the defect was found or initially created.
- CAUSED AT OP: The operation that caused the defect.
Initially, the value is same for both the fields. However, during the disposition process, you can choose to override the CAUSED AT OP field value if the operation that caused the defect differs from where it was initially found.
Follow these steps to modify the CAUSED AT OP field value:- Select the Perform Disposition
action button for the specific non-conformance number.
The Disposition Plan window appears, displaying the associated serial/lot(s) in the left pane.
- Select
to access the serial/lot(s) details.
Note:You can modify the value of the CAUSED AT OP field only when the defect is in Pending Disposition status. - Select
to modify the value in the CAUSED AT OP field.
Note:Only operations that are in the Complete or In Progress status will be populated in the drop-down list. - Select the operation from which the non-conformance originated or where it was caused.
- Select
to save the changes.
Refer to the method of disposition to perform the defect disposition for serialized and non-serialized lots.