Search for an Activity

Procedure

  1. Log in to Plant Applications Web Client.
  2. In the application navigation menu, select .
  3. If you want to search for a completed or a skipped activity, select Completed.
  4. Select .
  5. As needed, specify the search options within a specified start and end time.
    Tip:
    To search for an activity using a barcode, select for an option and scan for the barcode specific to the option. Use your device's front camera only for Barcode/QR code scanning. The application supports one-dimensional (Aztec, Data Matrix, MaxiCode, PDF417, UPC-A, UPC-E, UPC/EAN Extension) and two-dimensional (Codabar, Code 39, Code 93, Code 128, EAN-8, EAN-13, ITF, QR Code, RSS 14, RSS Expanded) types of standard codes.
    Note:
    In an iPad, you can use only in the Safari browser.
  6. Select Apply.

Results

The activities that match the search criteria appear.
Tip:
To clear results and perform new search, select Reset.