Access the History of an Operation

About this task

As an operator, you can access the events associated with an operation. An event is created each time the status of a serial/lot, operation, or the work order is changed.

Procedure

  1. Access the operation whose history you want to access.
  2. Select History.
    The History section appears, displaying the events associated with the operation and the serial/lot selected in the left pane. The events appear in the descending order of their timestamps (based on the TIME STAMP column). The following table provides information on the columns in the table.
    ColumnDescription
    ACTIONThe action performed on the serial/lot.
    SERIAL/LOTThe unique identifier for the serial/lot on which the action was performed.
    OPERATIONThe name of the operation for which the action was performed.
    USER(S)The name of the user who performed the action specified in the ACTION column.
    TIME STAMPThe date and time when the action was performed.
    Tip:
    To export the data to a .csv file, select . The data for the columns that appear in the table are exported into a .csv file. If the data contains unicode characters, to access the data in a Microsoft Excel worksheet:
    1. Access a blank worksheet.
    2. Go to Data > From text/CSV, and select the .csv file.
    3. Select the file origin: 65001:Unicode (UTF-8).
    4. Load the data.
    This process is a requirement for Microsoft Excel.