PRT_ASSOC
The PRT Item Association ( prt_assoc ) configuration file is used to define a parent-child association between a serialized and non-serialized item. Configure one record for every parent-child association to be made during production.
OPTIONAL FILE
The fields are:
| No. | Field Name | Description | Data Type | Entry Example | |
| 0 | region_id | Name of the region in which the parent-child association will take place. | 16 characters | PROCLNE2 _COM | |
| 1 | item_type_id | Unique name of the item type that will enter the above region (can be serialized or non-serialized). | 16 characters | WSHR_FRAME | |
| 2 | role-code | Code indicating the role of the item type as follows: | One byte | 1 | |
| 1 | Parent item (serialized) | ||||
| 2 | Child item (non-serialized item), | ||||
| 3 | Bystander (no association will take place) | ||||