PRT_REGION
The PRT Region ( prt_region ) configuration file is used to define every region in the Tracking Model.
REQUIRED FILE
The fields are:
| No. | Field Name | Description | Data Type | Entry Example | |
| 0 |
prt_svc_id
|
Specifies the PRT Data Collector Resident Process Service ID. This must be identical to the ID in service.dat . | 32 characters | APRT_DC | |
| 1 |
region_id
|
Unique name for the tracking region. | 16 characters | ASMBLY LNE1_NOR | |
| 2 |
region_desc
|
Textual description of the region. | 40 characters | Assembly Line 1 Normal Region | |
| 3 |
region_label
|
Text to display with the region for user recognition. | 16 characters | AssmblyLne1 Nor | |
| 4 |
tracking_type_id
|
Primary tracking region type: Pool, Detainment, Sequential or Shifting | 16 characters | SEQUENTIAL | |
| 5 |
region_cap
|
Maximum number of available physical region locations. | Integer | 15 | |
| 6 |
region_loc_cap
|
Maximum number of items that can reside at a single region location. Be sure to include all serialized and non-serialized items. | Integer | 3 | |
| 7 |
oos_cycle_count
|
Maximum number of items allowed to exit out of sequence from a tracking region. | Integer | 1 | |
| 8 |
oos_error_code
|
Indicates the action to be taken when an item does not arrive at the region exit transition indicator as expected. Use one of the following: | 8 characters | DLY_DTN | |
| DETAIN | Move to detainment region. | ||||
| SCRAP | Scrap (delete) item. | ||||
| DLY_DTN | Allow item to be out-of-sequence using the oos_cycle_count condition, then move to detainment region. | ||||
| DLY_SCRP | Allow item to be out-of- oos_cycle_count sequence using the condition, then scrap (delete). | ||||
| BLANK | (No item in the combo box) - Disable out-of-sequence. Used if the sequence of items entering a region is not important. This will scrap (delete) the item. | ||||
| 9 |
GEF_reserved_1
|
GE Intelligent Platforms Reserved. | 8 characters | Blank | |
| 10 |
GEF_reserved_2
|
GE Intelligent Platforms Reserved. | 8 characters | Blank | |
| 11 |
GEF_reserved_3
|
GE Intelligent Platforms Reserved. | 8 characters | Blank | |
| 12 |
GEF_reserved_4
|
GE Intelligent Platforms Reserved. | 8 characters | Blank | |
| 13 |
det_region_id
|
Unique name of the detainment region where items are sent when out of sequence. | 16 characters | DETAINMNT_A | |
| 14 |
region_lockable
|
Enable/disable (1/0) locked region, i.e. region must be locked to make modifications or to move items into the region. | One byte | 0 | |
| 15 |
alarm_det_region
|
Enable/disable (1/0) alarm generation when items are moved to the detainment region. | One byte | 1 | |
| 16 |
alarm_region_not
_empty
|
Enable/disable (1/0) alarm generation when a disperse tracking region is not empty and new items have arrived in the region. | One byte | 0 | |
| 17 |
alarm_region_lock
|
Enable/disable (1/0) alarm generation when an item enters an IN-LOCKED region or exits an OUT-LOCKED region. | One byte | 0 | |
| 18 |
alarm_loc_cap_excd
|
Enable/disable (1/0) alarm generation when the number of items at a single region location exceeds the configured maximum. | One byte | 1 | |
| 19 |
alarm_item_hold
|
Enable/disable (1/0) alarm generation when an item enters a region with an attribute that matches an item-hold specification. | One byte | 1 | |
| 20 |
alarm_unknown_item
|
Enable/disable (1/0) alarm generation when information cannot be retrieved for a serialized item. | One byte | 1 | |
| 21 |
enable_master
_alarm_flag
|
Enable/disable (1/0) alarming for this tracking region regardless of alarming enabled elsewhere. | One byte | 1 | |
| 22 |
enable_master
_log_flag
|
Enable/disable (1/0) logging for this tracking region regardless of logging events enabled elsewhere. | One byte | 1 | |
| 23 |
log_det_region
|
Enable/disable (1/0) logging when items are moved to the detainment region. | One byte | 1 | |
| 24 |
log_region_not
_empty
|
Enable/disable (1/0) logging when a disperse tracking region is not empty and new items have arrived in the region. | One byte | 0 | |
| 25 |
log_region_stat
|
Enable/disable (1/0) logging when an item enters an IN-LOCKED region or exits an OUT-LOCKED region. | One byte | 0 | |
| 26 |
log_loc_cap_excd
|
Enable/disable (1/0) logging when the number of items at a single region location exceeds the configured maximum. | One byte | 1 | |
| 27 |
log_item_hold
|
Enable/disable (1/0) logging when an item enters a region with an attribute that matches an item-hold specification. | One byte | 1 | |
| 28 |
log_unknown_item
|
Enable/disable (1/0) logging when information cannot be retrieved for a serialized item. | One byte | 1 | |
| 29 |
log_item_scrapped
|
Enable/disable (1/0) logging when an item has been scrapped (deleted) from the tracking region's queue. | One byte | 1 | |
| 30 |
log_item_entry
|
Enable/disable (1/0) logging whenever an item is entered into queue. | One byte | 1 | |
| 31 |
log_item_exit
|
Enable/disable (1/0) logging whenever an item exits the tracking queue. | One byte | 1 | |
| 32 |
log_item_mod
|
Enable/disable (1/0) logging whenever an item's tracking data is modified. | One byte | 0 | |
| 33 |
log_prod_start
|
Enable/disable (1/0) logging when tracking of an item starts in this region. | One byte | 0 | |
| 34 |
log_prod_stop
|
Enable/disable (1/0) logging when tracking of an item stops after this region. | One byte | 0 | |
| 35 |
item_qty_ptid
|
Point ID that displays the total number of items contained in the region; must be of type INT or UINT. | 55 characters | ASMBLYLNE1 _TOTAL | |
| 36 |
stat_ptid
|
Point ID that represents the region's status; must be of type UDINT. | 55 characters | ASMBLYLNE1_ STAT | |
| 37 |
region_type
|
Secondary tracking region type. Use the following codes: | Integer | 1 | |
| 1 | Normal | ||||
| 2 | Combine | ||||
| 3 | Disperse | ||||
| Note: If a Combine or Disperse region, region_cap field must be set to 1, and region_loc_cap must be greater than 1. | |||||
| 38 |
auto_assoc_region
|
Indicates if items are automatically associated in this region; must be of secondary region type Combine. Yes/No (1/0). | One byte | 0 | |
| 39 |
resource_id
|
Uniquely identifies the resource against which the alarm will be generated at the tracking region level. Note: If a resource is not designated here, the alarm will be generated against the default, "$SYSTEM." | 16 characters | OpWks_1 | |
| 40 |
cfg_override
|
GE Intelligent Platforms Reserved. | One byte | Blank | |
| 41 |
alarm_oos_region
|
Enable/disable (1/0) alarm generation when an "out-of-sequence" condition occurs. | One byte | 1 | |
| 42 |
alarm_inval_type
|
Enable/disable (1/0) alarm generation when an invalid item type enters the region. | One byte | 1 | |
| 43 |
log_inval_type
|
Enable/disable (1/0) logging when an invalid item type enters the region. | One byte | 1 | |
| 44 |
alarm_unknown_type
|
Enable/disable (1/0) alarm generation when an unknown item type enters the region. | One byte | 1 | |
| 45 |
log_unknown_type
|
Enable/disable (1/0) logging when an unknown item type enters the region. | One byte | 1 | |
| 46 |
alarm_reg_cap
|
Enable/disable (1/0) alarm generation when the region's configured capacity has been exceeded. | One byte | 0 | |
| 47 |
log_reg_cap
|
Enable/disable (1/0) logging when the region's configured capacity has been exceeded. | One byte | 0 | |
| 48 |
auto_move_point
|
Text Point ID that displays when an item moved into the region due to a "Point-based" move. The Point contains the item ID and optional information depending on the value of the num_setpt_param set in the global parameters files. | 55 characters | Blank | |
| 49 |
tran_region_id
|
Indicates the transition region ID for a shifting region. | 16 characters | Blank | |