Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Field Class / Description Property


Description Property (Field)
Description of the field.
Syntax
Public Property Description As System.String
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also