Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Field Class / Name Property


Name Property (Field)
The name of the individual field
Syntax
Public Property Name As System.String
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also