Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class
Fields Properties Methods


HistorianConfiguration Class Members

The following tables list the members exposed by HistorianConfiguration.

Public Constructors
Public Fields
 NameDescription
Public Field The current number of data stores configured.  
Public Field The current number of scada buffer tags.  
Public Field The current number of tags.  
Public Field The current number of active user connections.  
Public Field The last modification time of the collector configuration in a Historian server, expressed in UTC.  
Public Field The name of the last user to modify the collector configuration in a Historian server.  
Public Field The last modification time of the enumerated set configuration in a Historian server, expressed in UTC.  
Public Field The name of the last user to modify the enumerated set configuration in a Historian server.  
Public Field The actively licensed server features.  
Public Field Licensed duration for scada buffer data store in days  
Public Field The maximum number of data stores licensed.  
Public Field The maximum number of licensed scada buffer tags.  
Public Field The maximum number of licensed tags.  
Public Field The maximum number of licensed user connections.  
Public Field The version of a Historian server.  
Public Field The last modification time of the tag configuration in a Historian server, expressed in UTC.  
Public Field The name of the last user to modify the tag configuration in a Historian server.  
Top
Public Properties
 NameDescription
Public Property The product type of Historian.  
Top
Public Methods
 NameDescription
Public Method Converts the value of this instance to a System.String.  
Top
See Also