Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class / CollectorsLastModifiedTime Field


CollectorsLastModifiedTime Field
The last modification time of the collector configuration in a Historian server, expressed in UTC.
Syntax
Public CollectorsLastModifiedTime As System.Date
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also