Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class / EnumeratedSetLastModifiedUser Field


EnumeratedSetLastModifiedUser Field
The name of the last user to modify the enumerated set configuration in a Historian server.
Syntax
Public EnumeratedSetLastModifiedUser As System.String
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also