Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IEnumeratedSets Interface / Delete Method
Name of the set to remove.


Delete Method (IEnumeratedSets)
Delete an enumerated set from Historian.
Syntax
Sub Delete( _
   ByVal enumeratedSetName As System.String _
) 

Parameters

enumeratedSetName
Name of the set to remove.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also