Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IEnumeratedSets Interface / Unsubscribe Method
An existing set to Unsubscribe


Unsubscribe Method (IEnumeratedSets)
Clear any established enumerated set subscriptions.
Syntax
Sub Unsubscribe( _
   ByVal enumeratedSetName As System.String _
) 

Parameters

enumeratedSetName
An existing set to Unsubscribe
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also