Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IEnumeratedSets Interface / Rename Method
Existing set name.
New set name.


Rename Method (IEnumeratedSets)
Rename an existing set in a Historian server. Renaming a set does not make the previous set name available for use.
Syntax
Sub Rename( _
   ByVal oldname As System.String, _
   ByVal newname As System.String _
) 

Parameters

oldname
Existing set name.
newname
New set name.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also