Change the BOM Assignments of an Operation
Before you begin
About this task
Procedure
- Access the work order that you want to modify.
- In the upper-right corner of the page, select
, and then select Edit workorder.
The Edit <work order name> page appears, displaying a list of operations in the work order. - Select BOM.The BOM workspace appears, displaying a list of BOM items in the MATERIAL DESC column along with the details such as sequence, material, required quantity, unit of measurement, and number of substitutions in the SEQ, MATERIAL, REQ QTY, UOM, and SUBSTITUTIONS columns, respectively.
- In the OPERATION column, select the operation that you want to link to the BOM items. You can only select an operation that is not started. If the behavior of an operation is set to Non Clocking, the operation does not appear in the list.
- Select Save.The changes made to the work order are saved.