Advance a Process Order
About this task
Note:
Before you can manually advance a process order, the Schedule
Control Type needs to be set to Schedule Flows Independently on the
General tab of the Execution Path Configuration dialog box in the
Plant Applications Administrator.
Procedure
- Log in to Plant Applications Web Client.
-
Select
.
By default, the Open page appears, displaying a list of process orders grouped based on the multiple execution paths (configured in Plant Applications Administrator) in a tabular format - From the PATH filter, select the required execution path for which the Schedule Control Type is set to Schedule Flows Independently in the Plant Applications Administrator.
-
For a process order with a status of Active, from the Actions
column, select
for a required process order.
-
From the menu, select Advance PO Unit.
The Advance PO Unit window appears displaying active and completed units under the Active Completed Units section and available production units under Advance To Units section.
-
From the Advance To Units section, select the production unit that you
want to advance the process order to and select the OK button.
The selected production unit moved to the Active and Completed Units section.