Search for a Process Order

Procedure

  1. Log in to Plant Applications Web Client.
  2. Select .
  3. If you want to search for a completed or a skipped activity, select Completed.
  4. Select .
  5. Provide values in any of the available boxes as described in the following table.
    Box Description
    Execution Path Enter the name of an execution path.
    Process Order Enter a process order number.
    Product Code Enter a product code associated with the process order
    Select Dates Select this check box to enable Start and End Time entries. Using these fields, you can specify the time range by selecting the start and end times.
    Tip:
    To search for an operation using a barcode, select for an option, and scan for the barcode specific to the option.
    • Use your device's front camera only for Barcode/QR code scanning. The application supports one-dimensional (Aztec, Data Matrix, MaxiCode, PDF417, UPC-A, UPC-E, UPC/EAN Extension) and two-dimensional (Codabar, Code 39, Code 93, Code 128, EAN-8, EAN-13, ITF, QR Code, RSS 14, RSS Expanded) types of standard codes.
    • In iPad, you can use only in the Safari browser.
  6. Select Apply.

Results

The Process Orders that match the search criteria appear.
Tip:
To clear results and perform new search, select Reset.