Delete Process Order Comments

About this task

You can delete the comments made to a specific Process Order if security allows it.
Note:
You can modify or delete only those comments that were added by you. However, based on the site parameter, you can also update comments from other users if you have the required permissions.

Procedure

  1. Log in to Plant Applications Web Client.
  2. Select .
    By default, the Open page appears, displaying a list of process orders grouped by the associated execution path in a tabular format. You can select the Closed tab if you want to delete the existing comments of process orders that are in the completed status.
  3. From the Actions column, select for a required process order.
  4. From the menu, select Comment.
    The Add Comment page appears.
  5. Select for an existing comment.
    A confirmation message appears.
  6. Select Yes to complete the delete action.
    The selected comment is deleted for the process order.