Reset CouchDB Credentials
Procedure
-
You must define your configuration in the
silentinstaller.yml file. Update the following
parameter in the silentinstaller.yml file:
Parameter Description WEBCLIENT_INSTALLATION_PATH: "" Enter the Web Client Installation path in which you want to install. For example, WEBCLIENT_INSTALLATION_PATH: "/home/ administrator/install/" COUCHDB_SERVER: "" Enter the Plant Applications CouchDB host name or IP address. COUCHDB_USERNAME: "" Enter the CouchDB username. COUCHDB_PASSWORD: "" Enter the CouchDB password. - Access the utility.sh file in the plantapps-enterprise-webclient-<buildno> folder.
-
Provide execution permissions to utility.sh file by
running the following command:
sudo chmod +x your/pathto/installer/plantapps-enterprise-webclient-<buildno>/utility.sh
-
Run the
utility.sh
file by running one of the following commands:- If you are running this utility directly on the Enterprise Edition Web Client node:
<installer path>/plantapps-enterprise-webclient-<buildno>/sudo ./utility.sh -l -couch reset
- If you are running this utility remotely on the Enterprise Edition Web Client node:
<installer path>/plantapps-enterprise-webclient-<buildno>/sudo ./utility.sh -r -couch reset
Docker secrets are created based on the values you entered, and the Docker stacks are redeployed so that the containers use the new credentials. - If you are running this utility directly on the Enterprise Edition Web Client node: